VBUS.UVMODE

Description

VBUS.UVMODE sets what happens when the under voltage, UV, condition is detected. An under voltage is triggered:

When VBUS.UVMODE = 0, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH.

When VBUS.UVMODE = 1, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH and the controller attempts to enable the drive (software or hardware enable).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

VBUS.VALUE, VBUS.UVFTHRESH

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen VBUS.UVMODE 0x300A 0x4 USINT - - RW False